H106/... The new generation of standard hot runner systems
The new hotrunner manifold block H106/.... , like its predecessor Z106/..., is noted for its optimum melt flow and uniform heating. What is new is the use of the maintenance-friendly flexible tubular heating element Z 11381/... .
The new Pneumatic HASCO ejector coupling device, Z1680/...
Particularly with frequent mould changes, the coupling of the ejector system to the moulding machine accounts for a considerable proportion of the set-up time – and set-up time is cost-intensive downtime.
With the new pneumatic ejector coupling device Z1680/… from HASCO, this time can be significantly reduced. This reliable and compact powerhouse is activated pneumatically and reliably locks the coupling rod mechanically and without the continued assistance of compressed air.
Perfect solution for high-cavity moulds: Z3280/.../S Multimodule
The new Multimodule Z3280/... combines two to six modified Compact Shot nozzles Z3210/... in a minimum of space. Through the special modular design, it is possible to work with cavity-to-cavity distances that are unattainable with a conventional hot runner system. In addition, it offers a degree of flexibility in the arrangement of the gating points that a traditional multiple nozzle does not.

Deutsch
English
Espanol
Francais