Z 10650/... contourable gating insert
With the new xontourable gating inserts Z10650/... Hasco now offers you even greater desing scope for tunnel-type (submarine) gates.
HASCO has further extended its range of gating inserts and now offers even greater design scope for tunnel-type (submarine) gates with its new contourable gating insert Z10650/... .
The gating inserts are provided with an added stock and thus individually contourable, allowing direct adaptation to the contours of the mould.This results in new possibilities for the individual design of the moulded part.No evidence of the gate can be seen on the upper side of the part as a result of improved gate quality. The inserts are produced by the MIM process and made of highly wear-resistant hot-work steel 1.3343.They are available in three sizes.
The mould maker saves a considerable amount of time by using the gating inserts and
can rely on clean separation of the sprue.
download image:
Z10650_Presse.jpg (2400x1733, 290 KB)
file:
Z10650/... Gate insert, square, contourablecontact:
Im Wiesental 77
58513 Lüdenscheid
Germany