15.10.2011

New HASCO inclined sliding carriage Z18110/…

With its inclined sliding carriage Z18110/…, HASCO has recently launched the smallest mechanical, positively controlled inclined sliding carriage onto the market. Because of its small size, the Z18110/… opens up new possibilities in mould design. Access to awkward undercuts in the article is made possible by its compact design.

 

As far as its dimensions are concerned, the inclined sliding carriage is not much larger than a spring-mounted ejector, but has a number of outstanding advantages such as no subsequent spring when freeing up the undercut, and constant stroke combined with defined slide motion. Thanks to the compact exchangeable unit, the movement takes place only within the subassembly, preventing wear on and in the cavity. Precise demoulding processes without damage to the produced item are thus guaranteed.

 

The DLC coating on the surfaces of the slide guarantees optimum slip properties and prolongs the service life. Due to the coating, no additional lubrication is needed, which means that it is also suitable for clean-room use.

download image:

Z18110_Presse
Z18110_Presse.jpg (2126x1536, 144 KB)
 

file:

Z18110 /... Inclined sliding carriage, D/GB/F
 

contact:

Hasco Hasenclever GmbH + Co KG- Lüdenscheid
Im Wiesental 77
58513 Lüdenscheid

Germany


(++49) 2351 957-0
(++49) 2351 957-237
info@hasco.com
Order-E-Mail: order.de@hasco.com