NPE 2006 Chicago
At this year’s NPE, the biggest American trade fair for plastics processing, exhibitors from over 100 nations showcased pioneering innovations
from the fields of raw materials, injection moulding, extrusion and mould design.
HASCO also unveiled its new “Hot Base" concept for the first time. From engineering to the colour-matching of finished tools,
HASCO is therefore presenting itself as a competent partner that can project manage, design, produce and support complete
mould packages comprising mould construction, standards, additional working and hotrunner processing right through to the start of production.
For our customers, this means bundled expertise from a single source, a shortening in mould manufacturing times and global
service for demanding mould projects.
The “dart point” project was also unveiled as a global innovation. The first fully electrically-driven, 32-cavity needle
seizure system in the world produced dart points from POM in an impressively low cycle time. This multiple-cavity system
that is fully compatible with clean-room environments is ideal for customers from the fields of medical technology and food packaging.
For the first time at the NPE, the heated ZI215/... sprue bushing was unveiled to the American market. The external
dimensions of this nozzle match conventional Inch sprue bushes and can be installed into existing moulds with minimal
effort. By doing away with the solidifying sprue, material is saved and the cycle time significantly reduced.
This represents a significant productivity advantage through a HASCO innovation at an unbeatably low price.
Christoph Boueke, President of HASCO America, summarised the success of the trade fair: “We were totally
amazed by the quality and number of visitors to the HASCO stand. HASCO has shown very impressively that
we are the expert partner for mould construction, hotrunner and special processing for our discerning customers in North and Central America".
|
 |