HASCO Portal
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
HASCO Innovations at the MEX

The Moulding Expo (MEX) in Stuttgart is the new international trade fair for tool, pattern and mould making. Designed to be the main industry fair for the sector, the focus here will be on innovations and solutions for the future from 30.05. – 02.06.2017. 

HASCO is using this year’s MEX to present new, simpler and more agile options for tool and mould making. In Hall 6/Stand 6C58, HASCO will be presenting a large number of innovations, product improvements, application optimisations and new services.

In the field of mould base technology, for example, the application-optimised guide bushes with a circlip groove will be on display, together with the new, individually configurable nameplates for the identification of moulds containing the inventory number, product name, production date or storage location, for example. When it comes to lifting and moving moulds, the new attachment points conform to the highest standard. Extensions to product ranges in the heating/cooling field permit practically-oriented solutions for tool and mould making.

The HASCO hot runner specialists will be presenting the industry with a new, user-friendly electronic control unit. The clear development specifications here were: maximum reliability in production and maximum performance for minimal investment. And the result is certainly impressive. The comprehensive HASCO product portfolio now contains a consistently high-grade, high performance low-budget controller. A further highlight is the Vario Shot nozzle series already presented at K2016: 1 nozzle – 1000 possibilities.  At the MEX, HASCO is now presenting the system with the additional Type 40 nozzle size.

Alongside its stand at the MEX, HASCO offers rapid and simple access to the new HASCO developments and its complete product portfolio of more than 100,000 articles at www.hasco.com. Equipped with the latest features and possibilities, the portal provides 24/7 support to mould makers. 

Whether online or live at Moulding Expo in Stuttgart, a visit to the HASCO stand is certainly worthwhile. As an internationally leading supplier of modular standard components and accessories, HASCO ensures that mould makers and plastics processors can work more easily, more rapidly and more efficiently. The HASCO specialist advisers will be pleased to welcome you at the MEX in Stuttgart to discuss specific practical solutions and their implementation. 

Hall 6/Stand 6C58

Download:
Press release