Expansion of the range boosts flexibility | HASCO Portaal
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
juli 2020

K-Standards – Expansion of the range boosts flexibility

The HASCO modular system with its precisely machined K plates meets all the requirements of today’s modern mould maker. Around 1,500 additional variants drive our standardisation program, consequently further developing the tried-and-tested K program and at the same time increasing flexibility.

The new dimensions and variants have been specifically aligned to the individual requirements of the mouldmaking sector and precisely reflect the wishes of our customers, who have been involved in the compilation of the range right from the start.

The K standard parts, manufactured with high precision from low-tension European quality steel, are characterised by their modular structure and the variety of options. Customers also benefit from the system bores that have already been drilled. These are either designed to nominal dimensions for direct use or incorporate an allowance for subsequent heat treatment.


In addition to the precision and quality of the plates, HASCO places particular importance to their stock availability and short delivery times. As the first supplier of the full range of standard parts for mould making, HASCO's expanded K range offers an optimal combination of simplicity, availability and precision, thus permitting even greater cost efficiency.

More than 1500 additional dimensions and variants for the K-Standards are now available in the HASCO online shop.

Press release