HASCO Portaal
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
februari 2018

HASCO innovations at Metav, 20-24 February 2018

HASCO – the internationally agile supplier of modular standard components and accessories is presenting a large number of attractive innovations for tool and mould making at Metav, Hall 15/Stand D69.

Live presentations will be given on the stand of the new ejector configurator, which enables users to conveniently configure ejector pins in any desired lengths online, the new nameplate editor for the clear, customized labelling of different moulds, and also the machining of the new HASCO through-hardening steel 1.2714HH, which permits efficient work and hence time savings through its optimum, ready-for-use hardness.  

In the field of Mould Base Technology, innovative fastening devices like the load ring and rotatable eye screw ensure the highest standards for lifting and moving moulds. Additions to the range in the area of temperature control permit customised, practically oriented solutions for tool and mould making. Non-rotating ejector pins, flat ejector pins with two and four corner radii, adjuster plates for optimum pressure distribution and round, mechanical cycle counters, round latch lock units, stack mould components with a 2.5 module and new manifold blocks provide a well-rounded range of new components, with constant further additions enabling flexible applications.

Hot Runner Technology is presenting a new, user-friendly electronic control unit for the industry. This low-budget controller, which is both powerful and of a consistent high quality throughout, ensures maximum reliability during production. The Vario Shot nozzle series – "1 nozzle – 1000 possibilities" supplemented by the Type 50 nozzle size will also be on display at the fair. One particular highlight is the presentation of the new screw-in Vario Shot. This permits ready-to-mount systems designed and manufactured individually to customer specifications. Simple mounting and removal from the mould are guaranteed, as is freedom from leaks. Quick & Easy is the motto for the fully-mounted and electrically-wired hot runner system.

Another innovative further development for the HASCO app is the new cartridge heater calculator, permitting easy calculation of the individually required heating output. New features in the HASCO Portal provide 24/7 support for mouldmakers worldwide.

HASCO offers its customers rapid and simple access to all the new developments and its complete product portfolio of more than 100,000 articles via www.hasco.com.

Download: Press Release