HASCO模具标准
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
HASCO CAD data for SolidWorks®

HASCO customers will have a comprehensive database with native CAD data for SolidWorks®. The data is perfectly adapted to the needs of modern mould making. The considerable added value of the data enables users to benefit from significant time and cost savings, along with the complete mould making process. 

The speed and availability of CAD data for standard parts constitutes the basic prerequisite for the efficient design of moulds. Through this CAD data with its added value, HASCO is taking a decisive step forward and offering its customers further potential savings. The native data, generated in the original CAD system, features installation spaces, resulting in considerable time savings during the design process. The installation spaces can be included in the individual design with just a few clicks, together with the geometry that needs to be removed.

Native CAD data with installation spaces for the shortest design times

The fully parametric data also has decisive advantages if any changes are made, since the relevant parts automatically adapt to the corrections. The subsequent parts list that is then generated eliminates the risk of incorrect orders. The largely automated ordering process ensures punctual delivery for the start of assembly and rounds off the overall process in a perfect manner.

Installation manual


 

SolidWorks 本地数据库 - 从客户出发,为客户着想

David Nyström 在开发 SolidWorks 本地数据库中投入了大量工作同时运用了大量的设计窍门。设计师们可以借助参数,充分利用 HASCO 各种组件所带来的无限可能性。借助配置窗口,可简单地生成和改变模具结构。同样地,由于基本几何参数是确定的,可以非常容易地修改设计中所使用的各种配件。

借助宏,可以非常快速地创建模具顶料器

HASCO 标准中有超过 39,000 种配置均可以直接以 SolidWorks 本地数据库的数据格式提供给您使用。

所有这些在其主页下均可以免费下载。如您对此感兴趣,可通过以下链接进入网页。
www.bestmoldcomponents.com

另外,设计师的油管 (YouTube) 频道上,以及主页上的教学当中还可以找到相关介绍视频。